I am new to Automation Studio V4.9. I am getting a “License violation on target” status message when I hover my cursor over the Run Status shown at the bottom of my application. Any thoughts? How do we know what licenses are required?
I have Technology Guarding V1.7.1.1 and my coworker has V1.3.1.1 and we have different display behaviors when it comes to license status. His version shows that I needed 2 additional licenses than what was loaded on the dongle. My version appeared to be fine with the single license that I had and when I added the licenses that his system recommended the status on my version showed question marks implying it was not needed. Should I revert back to the older version of Technology Guarding or no?
I will add that when I added the 2 licenses that his system recommended then the “License violation on target” error did go away. But if I did not have my coworkers setup, how would I have known to add additional licenses?
Thank you for the response it is appreciated. I am very new at this software. Can you explain or point me to how I access this PLC logbook? Thank you again for your time.
you can open a browser and access the SDM (System Diagnostic Manager). For example, type 192.168.0.1/sdm into the address bar. Use the IP address of the controller.
B&R has modified its Licence Model now several times. The Technology Guarding tool was constantly updated to consider only the actual Licence Model.
Depending on the Runtime on the PLC it is possible that the Runtime is still unsing an older Licence Model.
If the system is operational , the best information is the Logger, like Stephan mentioned.
The Automation Studio does also provide access to the Logger.
Thank you for everyone contributing to this discussion. Currently we are still troubleshooting our setup. Technology Guarding shows that we have all of the proper licensing, but we are unable to jog 2 servos. We also have a Spindle application and that is running as expected. From what I have been able to gather from our lead programmer, it seems the CNC control is calling for a move, when the servos should be sitting idle and stopped. When we attempt to jog, I believe we get errors along the line that a move command is not allowed. Please excuse my terminology, as I collect more specific data.
We have several machines of this type functioning in the field, and we have copied these program configurations from these units. That’s when I started to investigate the licensing conflicts between my lead programmer’s older version of Technology Guarding claiming that I needed additional licensing. Since then, we have added the additional licenses (iTGMPCNC.02 & 1TGMPSPINDLE.O2 which both point to an alternative license 1TGMPFLAT.02) I am making an assumption that our system should run the same with the consolidated “xxFLATxx” license or both of the other licenses without an issue. Currently our ability to jog 2 servos is not functional and we are not sure why. Any advice or suggestions for support would be appreciated.
Please provide Information About used Version , Automation Studio, ACP10, ARNC0.
If there is an error in any Diagnostic, please provide Saved-File or Screenshot.
It may also be usefull to switch to a different Thread, as this will be more motion topic and less Licencing.
Thank you Michael & Valerio and others who have been contributing to the discussion. On yesterday we discovered that we had an “Abort” button was not wired properly (my fault) and since it was a NC button the system saw it as being pressed constantly since the circuit was open. Essentially the system interpreted that constant Abort as a stop command, not allowing a jog command to occur. I think what threw us for a loop was the fact a “motion active?” status bit was set even when first resetting the Estop. We would normally expect Motion active to not be active and so we went down the wrong path.
Thank you to all those that contributed. Our machine is running now.