Mapp Services 6.6.0 : the OPC UA Interface of MpAudit is disabled per default

Starting with mapp Services 6.6.0, the OPC UA Interface of MpAudit has to be explicitly enabled (disabled by default).

This has unfortunately been missed from the Revision Information. :cry:

image

Once this configuration property has been set to TRUE, MpAudit should behave the same as in version 6.5 (or lower).

4 Likes