Hello,
We are developing in mapp View 6.5 and I have created a simple SVG (below) with a path and no fill assigned.
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<!-- Created with Inkscape (http://www.inkscape.org/) -->
<svg
width="16"
height="16"
viewBox="0 0 4.2333332 4.2333333"
version="1.1"
id="svg1"
xmlns="http://www.w3.org/2000/svg"
xmlns:svg="http://www.w3.org/2000/svg">
<path
id="path"
d="M 0.52916664,0 H 3.7041665 C 3.9973248,0 4.2333331,0.23600832 4.2333331,0.52916664 V 3.7041665 c 0,0.2931583 -0.2360083,0.5291666 -0.5291666,0.5291666 H 0.52916664 C 0.23600832,4.2333331 0,3.9973248 0,3.7041665 V 0.52916664 C 0,0.23600832 0.23600832,0 0.52916664,0 Z" />
</svg>
When I assign this SVG to be the image embedded in a Button, imageColor correctly sets the fill of this path.
However, when I use this SVG in Image or ImageList, imageColor has no effect on the fill of this path.
In all cases, useSVGStyling is set to true.
Am I incorrect in my assumption that these three widgets should behave identically? Should I be using the Paper widget instead? That seems like overkill.
Thanks for any help!