MappCockpit Trace - Trigger condition - additional condition

With the trace integrated in Automation Studio, it is possible to define additional trigger condition using logical operators such as AND, OR, or XOR.

When using the trace in MappCockpit, a second “Start Trigger” can be configured. However, is there also a way to logically link both triggers?

Hello,

AS-Help mappCockpit Trace Configuration

It looks like the amount of trigger has been inreased from 2 (AS4) to 15 (AS6).
But i could not find any indication of a possibility of altering the combining logic from beeing pure “or” to something else.

I think you are already aware of the not so nice alternative to program this Trigger in your PLC code, which would then need a transfer for the application.


If nobody else comes up with an idea, you can combine these two Pictures with a Use-Case description to the local Sales contact of B&R to place a Product-Request. The Product Manager can then decide if he plans this improvement in a later version.

Greetings
Michael