Hello,
I have positive experience with mappCockpit (MC) from version 4.12, but I’m struggling with AS 6.5 despite following all the guides in the Help section and here on the Community.
MC is configured as follows:
enabled:
However, after opening MC and logging in, I have no connection to traces:
This is despite the trace being configured.
I also have no access to mapp components (mainly mappMotion):
This is despite the mapp components being up and running.
Can anyone help identify where the problem might be?
Thank you
Regards
Michal Malek
Update mapp Cockpit 6.3
Topics
Anonymous Login
Links to other Web-based Diagnostic Pages
Mapp Motion Axes - Commissioning View
Mapp Motion Configuration - Common View
Mapp Services - Common View
Integration of Online Help
1. Anonymous Login
In preparation for the Cyber Resilience Act (CRA) the System gets more and more locked. The Anonymous Login in mapp Cockpit can now be used to reduce login time while development or in Test-Applications.
[image]
If it was activated, it is important to…
I had the same issue in the past when I opened first time mapp Cockpit in AS 6:
Ciao
Valerio