Update mapp Cockpit 6.3
Topics
- Anonymous Login
- Links to other Web-based Diagnostic Pages
- Mapp Cockpit - Activate Extentions
- Mapp Motion Axes - Commissioning View
- Mapp Motion Configuration - Common View
- Mapp Services - Common View
- Integration of Online Help
1. Anonymous Login
In preparation for the Cyber Resilience Act (CRA) the System gets more and more locked. The Anonymous Login in mapp Cockpit can now be used to reduce login time while development or in Test-Applications.
If it was activated, it is important to disable the anonymous Login for productive Machines, to comply with the needs of the CRA.
Setting up the OpcUa Configuration
Login screen in mapp Cockpit
2. Links to other Web-based Diagnostic Pages
mapp Cockpit will become the central Hub for Diagnostics and offers links to other B&R Web-based Diagnostics. The links are only shown if a feature on the PLC is activated.
For Example Link to SDM
3. Mapp Cockpit - Activate Extentions
By default all mapp Cockpit Extentions are enabled.
If you switch to the Extended Visibility for Parameters in the Settings File, there are options to disable the Extentions.
4. Mapp Motion Axes - Commissioning View
There is a new more graphically aproach to present the Axes Data for Commissioning purpose.
Selection of new Commissioning Tab
The Commissioning Tab is only available for Axis which are operated via the McAcpAx-Library. Axis operated via other Libraries for example “PureVAx” does not show the Commissioning Tab.
Setup and Debugging of IO-Data and Communication
Presentation of Motor Speed-Torque Chart in mapp Cockpit
Setup and Debugging of Unit System
Setup and Debugging of Homing procedure
Presentation of movement Profile
Setup and Debugging of speed controller
Setup and Debugging of position controller
Move Sequence
This new Command enables the configuration of a movement Sequence to simpify the Test of the Control loop, by allowing to repeat positioning movements via one command.
5. Mapp Motion Configuration - Common View
We have now a Common View for the General mapp Motion Configuration.
This view can be used to see the Settings of a machine, and to manipulate for example the selective Logging settings during Runtime.
Selection of the Common View
Change Values during Runtime
6. Mapp Services - Common View
This View allows the user to operate the mapp Service functions out of the box.
Selection of the Common View’s for mapp Service
6a) mapp AlarmX
Set Commands and get Status via Watch Values
6b) mapp Recipe
Set Commands and get Status via Watch Values
6c) mapp PackML
Set Commands and get Status via Watch Values
7. Integration of Online Help
The integration of the online Help into mapp Cockpit has been started.
In the first step we provide a global Help Button which Links to the online Help.
Update mapp Cockpit 6.6
Topics
- Servo Loop Optimizer
1. Servo Loop Optimizer
The Menü for the Servo Loop Optimizer can now be opened on the Bottom of the Pages “Speed controller”, “Position controller”, “Feed froward”, which are part of the Commissioning Pages.
The Servo Loop Optimizer can be used to show the Frequency Diagram of the Control Loop. You can use the Filter Settings to optimize the Frequency Curve.
Half Screen Mode
Full Screen Mode
Greetings
Michael