Hello,
i use AS6.5 and MappCockpit 6.6.0
A new topic in MappCockpit is “Commissioning function” of axis.
Unfortunately, this function is not listed.
![]()
Hi @Bernard_Griot ,
for default that settings is not visible in the MappCockpit configuration file
I like a lot this post made by Michael about mapp Cockpit: Guide: Work with mapp Cockpit
Thanks
Ciao
Valerio
Hello,
The Commissioning Function is only available for ACOPOS Axis which use AcpAx Library, as far as i know. Which type of Axis did you use?
Greetings
Michael
Axis are listed in Mapp Cockpit but only with “Common”.
it is missing “Commissioning”
Hello,
The Reqired Library
is dependent on the Hardware you use. It could be that the requried Library is not yet part of LogicalView. Sorry if my question lead you to logical View but it is not the answer we looked for.
On which Hardware Implementaion is the Axis-Reference used?
In my Sample i have some Axes which support the Commissioning and one Axis which does not.
Check Logger for Informations or Warnings.
In the Logger you can see which kind of Axis is started and which libraries are used.
If there is a Library needed but missing, it will trigger an error.
Greetings
Michael
MappSafety 6.4.0 disturbs the Motion commissioning buttons..
Update your MappSafety to 6.4.1.
Thank you for your help!
Nice evening.