ERROR 427, Needed module mpcom of required range from V0.00 up to all higher versions not installed. 427

Hello, I’m getting an error and I couldn’t find the reason. ACP10 ARC0 version 5.25.1 is installed
mapp cockpit 5.24.2 installed. Can you help me how to solve this problem?

Needed module mpcom of required range from V0.00 up to all higher versions not installed. 427 C:\BrAutomation\sonproje\Binaries\Config1\X20CP1685\MpAxis.br

hi,

you need to select ‘mapp Motion’ instead of ‘ACP10 ARNC0(Motion)’ in ‘Runtime Versions’

When I do it this way, I get the mpaxis 5.21.2 mcXİS T.Y error. I am getting the error “It is not compatible with”. How can I solve it?

unfortunatley, we would need the project for that.

Go to menu ‘File’/ ‘Save project as ZIP without Upgrades …’

Hi @eem.ferhat Ferhat,

from my perspective your project looks well now. I can compile it.
Furthermore I added a simulation configuration and a mappCockpit configuration.

With the simulation your are able to do axis ‘commissioning’ with mapp Cockpit:

00.zip (9.5 MB)

Thank you.Where was my deficiency?

could compile it, so no big problems.
I just missed the mapp Cockpit configuration:

image

But let’s see what your real axis thinks about all this.
I could test the simulation only.