mpCNC error

we are using a 4 CNC mapp Axis and 1 non CNC mapp axis for the project (using MpCnc4Axis FB). but after controls on all the axis are healthy but getting CNC system error . I have mentioned AR and mapp version used, along with the log error for the reference.

AS Version - AS 4.3.11.134
AR versions - I4.26
VC Version - V4.34.3
ACP10/ARNCO - 3.18.2
mapp - 1.62.1

ver1

1 Like

Hello,
Please check if the ARNC0 init File has been set up with the correct Axis References.

To use an Axis with ARNC0 you have to enable it via “Additional Data” in the Mapping File
CNC_Enabled=“1”

In the InitFile you can then Reference to an Axis

Hello,
i may add this Link to the Documentation.

Documentation about Axis References - AS Help

Greetings
Michael

When that 1 non CNC axis is disabled the error was rectified and the project will be operational, but if enabled at that time, an error will occur again.

Hello,
Can you descripe your configuration more in detail. The Community can handle multiple Screenshots, you don’t have to spare. To get the whole Story out of an Logger entry is somtimes very hard.

For example show the position where you “enabled” or “disabled” the Axis, Configuration of your CNC-Init File, Axes Mapping File, …


Please be also aware of the dual Use Limit of the ARNC0 , with more than 4 Axis in a Group you would need a special Version. But as you mentioned the 5th Axis is non CNC. This should not be your issue.

Greetings
Michael

Hi @swasthikzetta,

It looks like you got some good suggestions from other community members, and it has been a couple of weeks since the last activity on this post. Can you please mark the reply that helped you the most as the solution? Or if you still have open questions on this topic, can you please provide an update?

Because there was no reply for a long time, the topic has been marked as solved. Feel free to return if you need further assistance, or mark the reply that helped you. Thanks