In 8LS motors documentation the (shared values or General values) section are not complete, where the Max. permissible output torque MK0 [Nm] and Max. permissible peak torque MKmax [Nm] can not be found since the motor is not initally provided with gearbox unlike the 8LV motors. In case of adding a gearbox such as 8GP to an 8LS motor, those values can be calculated as following:
Mkmax = the maximum torque of the motor * gear ratio (Mmax * gear ratio)
For Mk0 the standstill torque (M0) needs to be used but for the dT60 curve (yellow in the attached picture) as there is derating of the nominal values from the motor when a gearbox is attached. Therefore,
Mk0 = (M0 dT60 * gear ratio)