Hi community, I’m currently using the AsMbTCP library to establish a connection between a PLC and an IPC, but I’m having trouble connecting. I’m wondering if I need to declare and use a modbustcp_any block in the Physical view if I’m using this library? Also, how do I know if the PLC has successfully communicated with the IPC? I used my laptop to ping the command prompt and send Modbus signals via the Modbus Poll application, and I was able to connect and send signals to the IPC, but my PLC wasn’t connected. I also looked at the LibAsMbTCP1_ST library to build my code, but it still can’t connect or send signals. Can anyone help me find the problem?
ACTION Act_Communication:
IF gRobotEM.Command.Cntrl_Mode = 1 THEN
temp_DINT := 1;
ELSIF gRobotEM.Command.Cntrl_Mode = 3 THEN
temp_DINT := 4;
ELSE
temp_DINT := 0;
END_IF;
mb_WriteBuffer[0] := DINT_TO_UINT(temp_DINT AND 16#FFFF);
mb_WriteBuffer[1] := DINT_TO_UINT(SHR(temp_DINT, 16) AND 16#FFFF);
CASE gRobotEM.Command.Cntrl_StateCmd OF
pmlSTATE_RESETTING: temp_CntrlCmd := 1;
pmlSTATE_EXECUTE: temp_CntrlCmd := 2;
pmlSTATE_STOPPING: temp_CntrlCmd := 3;
pmlSTATE_HOLDING: temp_CntrlCmd := 4;
pmlSTATE_UNHOLDING: temp_CntrlCmd := 5;
pmlSTATE_SUSPENDING: temp_CntrlCmd := 6;
pmlSTATE_UNSUSPENDING:temp_CntrlCmd := 7;
pmlSTATE_ABORTING: temp_CntrlCmd := 8;
pmlSTATE_CLEARING: temp_CntrlCmd := 9;
ELSE temp_CntrlCmd := 0;
END_CASE;
mb_WriteBuffer[2] := DINT_TO_UINT(temp_CntrlCmd AND 16#FFFF);
mb_WriteBuffer[3] := DINT_TO_UINT(SHR(temp_CntrlCmd, 16) AND 16#FFFF);
IF (temp_CntrlCmd <> old_CntrlCmd) AND (temp_CntrlCmd > 0) THEN
cmd_PulseActive := TRUE;
ton_CmdPulse.IN := FALSE;
old_CntrlCmd := temp_CntrlCmd;
END_IF;
ton_CmdPulse(IN := cmd_PulseActive, PT := T#300ms);
IF ton_CmdPulse.Q THEN
cmd_PulseActive := FALSE;
ton_CmdPulse.IN := FALSE;
END_IF;
mb_WriteBuffer[16] := 0;
IF (temp_DINT > 0) AND (temp_DINT <> gExtInterface.PLC_To_Ext_Mode) THEN
mb_WriteBuffer[16] := mb_WriteBuffer[16] OR 16#0001;
END_IF;
IF cmd_PulseActive THEN
mb_WriteBuffer[16] := mb_WriteBuffer[16] OR 16#0002;
END_IF;
mb_WriteBuffer[17] := 0;
IF gHmiGlobal.Station.Cmd_ChangeRecipe THEN
mb_WriteBuffer[17] := mb_WriteBuffer[17] OR 16#0001;
END_IF;
IF gHmiGlobal.Robot.Cmd_Reset OR gHmiGlobal.Station.Cmd_Reset THEN
mb_WriteBuffer[17] := mb_WriteBuffer[17] OR 16#0002;
END_IF;
mb_WriteBuffer[18] := 101;
mb_WriteBuffer[19] := 0;
temp_UDINT := DINT_TO_UDINT(gCurrentRecipe.RecipeID);
mb_WriteBuffer[20] := UDINT_TO_UINT(temp_UDINT AND 16#FFFF);
mb_WriteBuffer[21] := UDINT_TO_UINT(SHR(temp_UDINT, 16) AND 16#FFFF);
CASE (instruction) OF
1: (* LỆNH ĐỌC *)
mbReadInputRegisters_0.enable := 1;
mbReadInputRegisters_0.pStation := ADR(ext_station);
mbReadInputRegisters_0.startAddress := 0;
mbReadInputRegisters_0.nrRegisters := 35;
mbReadInputRegisters_0.pData := ADR(mb_ReadBuffer);
mbReadInputRegisters_0.dataSize := SIZEOF(mb_ReadBuffer);
mbReadInputRegisters_0();
IF (mbReadInputRegisters_0.status <> 65535) THEN
fub_status := mbReadInputRegisters_0.status;
check_status := TRUE;
instruction_ready := TRUE;
IF fub_status = 0 THEN
gExtInterface.PLC_To_Ext_Mode := UINT_TO_DINT(mb_ReadBuffer[0]) OR SHL(UINT_TO_DINT(mb_ReadBuffer[1]), 16);
temp_DINT := UINT_TO_DINT(mb_ReadBuffer[2]) OR SHL(UINT_TO_DINT(mb_ReadBuffer[3]), 16);
gExtInterface.Ext_To_PLC_State := temp_DINT;
gExtInterface.Ext_IsRunning := (temp_DINT = 6);
gExtInterface.Ext_IsError := (temp_DINT = 8) OR (temp_DINT = 9);
gCurrentRecipe.RecipeID := UINT_TO_DINT(mb_ReadBuffer[32]) OR SHL(UINT_TO_DINT(mb_ReadBuffer[33]), 16);
END_IF;
A
END_IF;
2: (* LỆNH GHI *)
mbWriteMultipleRegisters_0.enable := 1;
mbWriteMultipleRegisters_0.pStation := ADR(ext_station);
mbWriteMultipleRegisters_0.startAddress := 0;
mbWriteMultipleRegisters_0.nrRegisters := 22;
mbWriteMultipleRegisters_0.pData := ADR(mb_WriteBuffer);
mbWriteMultipleRegisters_0.dataSize := SIZEOF(mb_WriteBuffer);
mbWriteMultipleRegisters_0();
IF (mbWriteMultipleRegisters_0.status <> 65535) THEN
fub_status := mbWriteMultipleRegisters_0.status;
check_status := TRUE;
instruction_ready := TRUE;
END_IF;
END_CASE;
IF (check_status) THEN
IF fub_status = 0 THEN
gExtInterface.IsConnected := TRUE;
robotAlarmCode := 0;
ELSE
gExtInterface.IsConnected := FALSE;
robotAlarmCode := UINT_TO_DINT(fub_status);
END_IF;
check_status := FALSE;
END_IF;
IF (instruction_ready AND fub_status = 0) THEN
CASE (instruction) OF
1: instruction := 2;
2: instruction := 1;
END_CASE;
instruction_ready := FALSE;
END_IF;
gHmiGlobal.Robot.ActualSpeed := gExtInterface.Pick_Rate;
END_ACTION