OfflineCommissioning parameters at Runtime Utility Center (AS6.3)

Hi all,

I have a question regarding new command OfflineCommisioning at RUC in AS6.3, this command is a successor of OfflineInstall, but i cannot define a relative path at offlineCommisioning at the PIL file.

Before i generated the CFast card with command(with Automation Studio 4.12.6):
OfflineInstall “.\CF0\RucPackage_APC_KSBxXR_S5.zip”, “KeepPermanentMemory=0”,

Now i want to generate also with relative paths:
OfflineCommissioning “.\test\RUCPackage_0\RucPackage_APC_KSBxXR_S5.zip”, “CompactFlash”

but this command is not accepted, only absolutely are accepted :frowning:
OfflineCommissioning “C:\01_Data\Prj\KOSME\KSBxR_S5\trunk\R8_4\Setup\CPU_S5\test\RUCPackage_0\RucPackage_APC_KSBxXR_S5.zip”, “CompactFlash”


Best regards
Marcin

Hello,
this is a known issue and already reported to B&R development
Lets wait for a fix :slight_smile:
best regards
Oliver