Problem: When reprograming a C50 and HW version 1.1.8/1.2.0 is selected and Terminal LX version is 1.0.1/1.1.1 /1.1.2, then the terminal is stuck in the loading screen. Basically the HW version 1.1.8/1.2.0 is not backwards compatible with older terminal versions (1.0.1/1.1.1 /1.1.2). The termonal is temporarily unresponsive with terminal USB port and Visu not showing. HW 1.1.7 still works with the older LX versions (1.0.1/1.1.1 /1.1.2.). The new IO data points “Terminal Memory Total” and “Terminal Memory Available” introduced in HW 1.1.8, causes this issue.
If you don’t know this issue it can cause major confusion on-site when updating a C50 or C80. Possibly also T-series panels.
Fixing the Stuck Terminal: Downgrade the HW version and do a USB installation. LX version cant be updated in this state as terminal USB does not work anymore. After the HW downgrade the LX version can be updated, then update the HW version and do USB install.
Workaround 1 : User always has to update terminal LX first and then the HMI program. This is not fool proof.
Workaround 2: Remove the new IO datapoints “Terminal Memory Total” and "Terminal "Memory Available from the HW file (HWx) . Be sure to create a new HW version Ex. make 1.2.0 a new version 1.2.1 with the removed IO data points. HW version file can be found in directory “C:\BRAutomation\AS412\AS\Hardware\Modules\PPC50xxxxx”
Make new version
Delete IO Data points
Use new HW version
I hope this helps someone! Feel free to ask a question if anything is unclear.