OPCUA node sets not available, - Tutorial for 6.3

Hi,

I am comparing projects in 4.2 and 6.3. I cannot get the UA Objects/nodes in 6.3 to properly display and be used as in 4.2. At this point I believe the two programs are configured identically (of course the settings are in different locations/removed/added) but I cannot seem to find why my test “machine” interacts with the 4.2 plc while connects to the 6.3 but cannot find/change the data i am trying to manipulate (a simple heartbeat master and heartbeat copy where the PLC changes the master, and the machine copies it).

I would like to try starting completely from the beginning in 6.3 and seeing if I have missed something? Or have other people faced similar issues with .uanodeset files or any learning curves in this transition period?

My debugging strategy has been to just have the 4.2 and 6.3 projects open, and simulate one, confirm some settings, turn it off, then simulate the other, and confirm it is still not working. I am completely stuck at this point and have even copied the .uanodesets and URIs directly from the working project, permissions as well as declaring the “Value Attribute Of” exactly.

Additional Info: I can see the PLC and nodes via UaExpert, I can see that the 4.2 project has the heartbeat copy manipulated, but the 6.2 does not, additionally the binding to the node is not present and I can only view the heartbeat I enabled in the .uad

Tbh I have no idea what is your problem :slight_smile: maybe you can add some printscreens to your description to make it more clear?

closed due to inactivity

Are you having the same problem I’ve described here? If you’ve found any solutions in the meantime, please post them.