Plaseholders mapping in AS 3.0.90

image
I need to work with an existing project in Automation Studio 3.0.90. How can I find the location in the code where the placeholder (like this {variable}) is referenced?

Hi,

I’m not 100% sure, but the screenshot looks like it’s out of a Visual Components 4 (VC4) visu, right?
If yes, there’s a so-called “text snippet” used. The snippet itself has a unique name (in your example: ErrNrStapler), and the datapoint is referenced in the configuration of that snippet.

Unfortunately I don’t have a suitable project available to lead you directly to the position of such a configuration, but please check Automation Help here for more details about text snippet configuration.

Hope that helps a bit, best regards!