Plug license dongle into USB port of P3 drive system

Hi guys

Does anyone know if it is possible to plug a license dongle into a P3 drive system?
We deliver optional axes to the client and need licenses for this, and don’t want to tell the support to add a license manually onto the main dongle plugged into the APC.

Thanks
Patrick

Hello,

According the help (see note 4) to X9 connector) it’s not possible.

Hey Pavel
Thanks for the swift answer.
I guess I then need a different approach to licensing management.

Have a great day
Patrick

Hi,

I want to add: While the port uses an USB connector, it’s not a USB interface at all in regards to the signals going through there. This is the reason for the limitation to only using the display - it’s using the same interface.

Best regards