Power Panel 35 : Error code 800041000 during power on

Witam

Szukam informacji o kodzie błędu 800041000
dla Power Panel 35
Dioda led STATUS świeci się na czerwono co świadczy o jakimś błędzie. Na wyświetlaczu po załączeniu zasilania pojawia się tylko:
Version: 1.1
Status: 800041000
Co to może być?

Hi and a warm welcome,

I am looking for information about the error code 800041000
for Power Panel 35
The STATUS led lights up red which indicates some kind of error. On the display after power on, it only shows:
Version: 1.1
Status: 800041000
What could it be?

Link to PP35 Manual

I am not aware that PP35 show builtin error codes on its display.
At least I didn’t find anything about this in the documentary.

The logger should show some infos about the error.

Best Regards,

Yes I read documentary yesterday but I can’t find anything els. Status 800041000 should say something but I don’t know what.

Many greathings for traing help

Can you provide a picture of the error? Is it an error from the panel or from the visualization?

yes, my first thought was also that it was the visualization. But since the red LED is lit, the panel is either in ‘SERV’ or in ‘DIAG’. The visualization should not be working there.

Error is on the panel

I was curious and sent a PP35 into the ‘DIAG’ via the node switch:

so reading out the logger would be more helpful.

Service Mode - What is it and how to collect diagnostics - Share Info & Ideas - B&R Community

Okay, cool. So we are closed. Please follow the post from @christoph.hilchenbac and try to read the logger. Share it with us (a screenshot with the error and details would be enough).

@Wojtek, what is the status of your question, have you resolve it?