Power Panel 65

4PP065.0571-P74 may know is this item already discontinue?

If yes what the new replacement part without re-does the HMI program?

Thanks

TM Tan

Hello,

Yes, the 4PP065.0571-P74 has already been discontinued. You can always check the LifeCycleStatus yourself on the B&R website (login required).

Unfortunately, there is no 1:1 replacement product for the PP65 available.

Hi,

You can use the 4PPC80.0573-10A.

The aspect ratio is the same as the PP65. The display resolution is higher, but if you enable “Local window scaling” in the terminal configuration, it will scale automatically. No changes are needed in VC4. It has the same cutout dimensions (188 × 130 mm).

Good hint from @jchmelik, so @Tzyy_Mei_Tan, do you have at least the project? So, is hardware replacement possible? If so, it is definitely possible to find new hardware and make your project run with minimum effort.

Closed by moderator due to inactivity.

For others, if you want to help from the Community, you have to continue the discussion and update the status of your progress. Otherwise, it is hard to help you.

Hi Kovar,

I am waiting customer reply to confirm for the replacement. If have any progress sure i will update here

Thanks

TM Tan