Albin
(Albin Magnusson)
September 24, 2026, 9:46am
1
Hi,
I am trying to localize the text for the HMI of an application I am developing but I am running into issues. I’ve never done this before so excuse my ignorance.
As you can see when I open my tmx file, LocalizableTexts.tmx I only have en de and fr to select from. I have configured many more languages, see the highlighted ProjectLanguage.
I used the language toolbox in order to add the languages, and I only have one design language selected (english).
I have also created a textconfig file in the configuration view. But I cannot select target langues from there, nothing shows up in the menu.
Does anyone have a clue what I might be doing wrong?
I am using the following versions:
Automation studio: 6.5.3.11
Automation Runtime: 6.78
Visual Components: 6.0.0
mapp Services: 6.7.1
OPC UA C/s: 6.7.0
mapp VIew: 6.7.0
mapp Cockpit: 6.3.1
Thanks in advance.
Samuel
(Samuel Otto)
September 24, 2026, 10:43am
2
Hi Albin,
welcome to the community!
Could you please provide a screenshot from the textconfig in the Configuration view?
BR, Samuel
Albin
(Albin Magnusson)
September 24, 2026, 10:57am
3
Thank you
Here is a screenshot of the configuration file:
As you can see I cannot select a target language. The tmx file I created shows up however.
we have a post for similar topic and step by step example: Using ArTextSysGetText() with C
I hope it helps
Ciao
Valerio
Samuel
(Samuel Otto)
September 24, 2026, 11:14am
5
In my case it worked without issues - tested with AS 6.7.0.
I simply added two new project languages to Project.language in LV and it is available in the .tmx files. Maybe delete and add these two files?
Albin
(Albin Magnusson)
September 24, 2026, 12:11pm
6
That is strange, I have tried to delete and create the files and sadly it did not solve the problem.
Albin
(Albin Magnusson)
September 24, 2026, 12:37pm
7
I got it to work. The problem was that the projectlanguage was nested in a data object. When I moved it outside it worked. I put it there because I had misunderstood
the automation help.