Texts in AS6

Hello,

I have problem with localizable texts. When I try to assign text over “system window - picker”, it’s empty! When I write the text directly to propertis, it show text in property ($…). In runtime show text from tmx in all languages right.

I try it before, when I start with project, it’s not show. After 3 times of removing and adding all project languages files, it show dialog correctly. But now it’s empty.

I have another project (older files version) and i’ts show correctly.

I use 6.3.4.31 and all newest packages.

Hello,
this issue is being resolved at local B&R office.

Hi @NovotnyJ and @tomas.travnicek, what is the status of this topic, can you update us and maybe it close it?

Hi @kovarj ,
You can mark it as resolved I believe. We are waiting for response from support, though. Once we receive new information I will write a comment here in this thread.

Hello

I have exactly the same problem

Since I convert my project from 4.12.8 to 6.5, I lost the text system

I asked the local support (BE), but they don’t have the problem on there PC running same AS6.5

My project converted seems Ok for support.

I un-install / re-install AS6.5 more than 10x using many way (AdminByRequest… IT admin… VM full admin…) but still the same

The strange things, when I compile, I get no error and I get correct display !!!

But now, I can not edit pages !

Can you help me ?

Thanks and regards

Marc

@tomas.travnicek do you have something you can share with us?

hi @Marc_Pinchart,
thank you for sharing your experience on this topic. It seems that more and more people are encountering the same issue. Currently, it is still under investigation and being addressed by B&R. I will update this topic as soon as I receive new information.
thanks @kovarj for reminder.

Thanks for your support

Additional information:

I install AS6.5 on :

  • a VM full admin
  • another laptop full admin (private)

The result is the same : no text link

But, during lots of try, i get strange behaviours:

(one time only) When i remove/reinstall “TextSystem” for the 10 times, suddenly, I get the texts appearing !

I close AS6.5, re-open: texts disappears ! … I can not reproduce this !

Marc

Hello

UPDATE

I think, I found the problem !

When I switch the “OPC UA C/S” runtime version from 6.5.0 to 6.0.0, the text system is back to normal !!

I do the opposite test (6.0.0 => 6.5.0) , the text system FAIL.

Note: you need to close/reopen AS to get the proper result

Regards

I marked your answer as a solution (I mean workaround).Still waiting for final solution from R&D team of course.

Thanks so much @Marc_Pinchart for your time for finding the cause of the problem.
Ciao
Valerio

…and additional info

I do the same test with OPC UA C/S (on Laptop and VM)

6.3.1 => fail

6.4.0 => fail

Back to 6.0.0 => Ok

May be some security/access right change between 6.0.0 and 6.x ??

Some colleagues get exactly the same behaviours ! .. they go back to 6.0.0

Hi,

I know this is a long stretch but could you try the following test.

  • Download AS6.5 ZIP file

  • Right click on the ZIP file

  • Under security check the box in the image

  • Unzip the file

  • Run installation for AS6.5

Ok

But where can I download the AS 6.5.5 ZIP ? :slight_smile:

There is only 6.5.0!

Thanks

Marc

Sorry the image is misleading because I converted it from german to english with ChatGPT :slight_smile:

Version 6.5.0.306 is the latest

Hi,
just received information from Support, fix ‘ll be available in AS6.5.1 and AS6.7.0
It was a rather rare issue dependent on the installed and used technology packages.
Thank you all for sharing your experiences!

Tom