PVIManagerAsService Silent/automated Installation not working

Hello,

i am trying to install only PVIManagerAsService with a PVI.ini and CMD Script, but it isn’t working sadly. I don’t really need the other components like PVI Monitor or Runtime utility center. The Version that i’m trying t install is is 4.7.2.30 because we need that Version.

that’s how the PVI.ini looks:

The PVI.ini is in UTF-8 coded.

and that’s my Script for it:

“C:\PVI_Manager\4.7.2.30\Setups\Automation Net PVI V4.7.exe” /S /O=“C:\Temp\pvi.ini” /L=1031

image

that’s the Service it is installing, but i am missing the PVI Manager Service after the installation.

Can someone please help me to install just that one component?

Hello Christian,

would it work if you did not install PVI via the command line, but instead ran the setup directly?

Best regards,
Stephan

Silent Installation of PVI - Ask Questions / HMI & Visualization - B&R Community

Hello Stephan,

Thank You for the quick reply.

yes that works well, the Service appears as B&R PVI Manager. But the thing is i really need it to be automated via Script.

I’ve looked that Article up, but it doesn’t work for me

Hello,

my pvi.ini file appears as follows:

[PVI]
PVIManagerAsService=0
RUC=1
TGDongleDriver=1
USBDongleDriver=0
CANDriverCC770=0
CANDriverSJA1000=0
OPCServer=0
PVIAPI=1
PVIHelp=1

i tried your PVI.ini file but it still doesn’t work.

Hello,

Could you please include a log file? Perhaps the issue will be visible in the logs.

“C:\PVI_Manager\4.7.2.30\Setups\Automation Net PVI V4.7.exe” /S /O=“C:\Temp\pvi.ini” /L=1031 /Log=C:\Temp\InstallationProcess.txt

Hello Stephan,

here is the content of the Log file:

Error: The parameter /Log cannot be specified with the parameter /S because logging is not possible in silent mode. (Error number = 4718)

Hello Christian,

please test the process without enabling Silent Mode.

Hello Stephan,

Without silent mode, I have to select which components I want to install. That defeats the purpose of what I’m trying to do.

However, I sent you a log anyway, with the default installation.

Installation Process.pdf (66.6 KB)

Hi @Christian_Fanea, please get in touch with local support. They can analyze your logger.