Software installation with PVI

Hello everyone,

can anyone help me find a solution to this problem?

I would like to know if there is a possibility to create a portable PVI package and run a .pil file on a laptop without installing any version of PVI manager or AS.

Thanks

Hi,

you first should create a RUC package:

B&R Online Help

and then ‘Create an installation package’ with the Runtime Utility Center:

image

B&R Online Help

using this button

RUC will then pack all necessary files including the dlls in the given folder.

(As you can see from the icon, an ‘installation CD’ was created in the past which afterwards could be handed out to e.g. service technician to install the PLC)

Thanks for the solution! It seems to work but there is only one thing: after creation I added the RUC.Net.Guard dll copied from the PVI folder to the package to make it work otherwise the package crashes.

Hi Gianluca @Gianluca_Puleo ,

I tested it with Runtime Utility Center V5.6.2.3 from PVI V4.12.6.86 and this DLL is present: