frogman
(Hansol Lee)
April 9, 2026, 9:32am
1
I am using an apc4100 (UEFI Boot) and installed the Hypervisor via USB. AR is working fine and it is also functioning well as a PLC, but when I checked the partitions in Disk Management, they are not partitioned and remain as Unallocated. Why is that?
I installed it by referring to the link below. The installation was done under the AS6 environment.
HypervisorInstallationGuide_WindowsV13.pdf (1.0 MB) v1.3
Versions
Version
Date
Comment
Edited by
1.0
Oct 7, 2019
First Edition
Brittany Langston
1.1
Oct 16, 2019
Indicated AS4.7 improvements, improved AHCI driver update section
Brittany Langston
1.2
Nov 14, 2019
Updated minimum BIOS requirements
Brittany Langston
1.3
June 7, 2022
Moved system requirements into document. Moved troubleshooting and FAQ to appendices. Validated accuracy of document.
Chris Hairston
1 Introducti…
Hello,
i am not an Expert on Hypervisor, but i try to understand your request…
As far as i understood you are not seeing the same situation like shown in AS-Help for the Partions after installing Hypervisor.
Partions for Hypervisor shown in GPOS
Did you do a full restart of the whole system?
Which image of partitions do you get?
Greetings
Michael
Hello,
I think i should have read the help more in detail. Could this sentence be the solution?
Greetings
Michael
frogman
(Hansol Lee)
April 9, 2026, 10:30am
4
Thank you! I think this explanation is correct. So it is normal that the partitions are not visible.