Dear All,
I am reaching out to you guys for some valuable inputs to a task I am dealing with. I have limited knowledge of IO link communication. I want to read SICK OD2000 sensor values thought X20DS538A module. The IO link module is installed, Sensor is plugged in, IODD files are installed using DTM configurator, DTM server is enable, FDT catalog is updated. However, I am still not able to connect with sensor because an error keeps popping up
IO link module configuration is a follows:
Additionally, status LEDs of X20DS438A module is:
r: Green i.e. Device is in OPERATE mode
C1: green/red (blinking as single flash) i.e. IO link communication is failing
Q1: Orange (stable): i.e. there is data traffic on the C/Q line in SIO mode
when I check Diagnostic error then there is Hardware error
This is the first step I am stucked into. Once it will be up running I will need to read data from sensor.
Will appreciate your input to that.
Many thanks in advance.