Replacement apc910

Is there an APC that has 5 PCI bus slots besides the APC910? because the APC910 is no longer in production, and the APC4100 only has 3 PCI bus slots for maximum

Hi Rijaluddin

Thanks for your message. Currently we only have 1 APC type that supports 5 PCI(e) bus slots and this is APC910. APC910 is still in production but will soon go into classic phase, meaning it’s not recommended for new developments.
APC4100 currently is not planned with 5 PCI slots as far as I know.

Jan

So the APC910 is still available? This is not a new use, it’s just needed for backup, 3 APC910s, because the slots needed are 5 slots, if you replace them with slot 3 I think it will be difficult

Yes for sure, you can still order it. If you’re running Windows, I’d recommend to ask for W10 2021 as the support for W10 2016 will discontinue soon (by Microsoft).
Take not that this will be the APC910 with the TS17-xx cpu boards, TS77-xx cpu boards are discontinued.