S120 Acyclic communication with B&R soft PLC

Hello, I am working on S120 drive from Seimens with B&R soft PLC and trying to establish acyclic communication using profibus. Can anyone help me with procedure?

Hello Ajay,

welcome to our community!

what is an S120?
what hardware does your B&R Soft PLC run on?

Gruß
Stephan

Hello Stephan,

Thanks, S120 - is siemens drive. Attached is the hardware.

Hello Ajay,

With the library AsNxDpM you can set up acyclic communication. See function block nxdpmxxxxWrite.

B&R Online Help

Hello Stephan,

I have checked the plc code, As per the code, I am already using this library for the both for the class c1 and c2 (functions are declared but not used). I would like to understand if I can use both kind of the communication/ blocks together.

Could you also please help me, How the normal flow of the program works in B&R?

Hello Ajay,

In order to read or write the data, the master (X20IF1061-1) must be operating a cyclic data connection to the S120 and the slave must support the DP V1 extension of the PROFIBUS standard. Please note that the X20IF1061-1 does not support DP-V2. Why do you want to use Class 1 and Class 2 acyclic communication at the same time?

Gruß
Stephan

Hi @er.ajaisharma10 ,what is the status of your topic, can you update us with your solution?

Hello Jaroslav,

I am working on the Siemens S120 side and after the testing of the solution. I will update.