Will there be a Win11 Support for safeDESIGNER?
SafeDESIGNER’s compatibility with Windows 11 is currently under investigation. Until now no limitations or incompatibilities are known but the full evaluation is not completed and no official compatibility declaration can be made, yet. A final statement is expected by end of 2024.
As a temporary workaround, a VirtualMachine with supported OS is recommended. Be aware of VM with project stored on shared drive on host machine does not allow download from RemoteControl
Based on Oliver’s reply, I would say you can try to use it. The statement that it is not officially fully tested and supported does not mean that it won’t work for you
Operating SafeDesigner on a not officially supported Windows version means operating SafeDesigner out of specification which then means that the chain of safe products is interrupted
This can result in serious legal issues if an accident is happening
My answer was to clearify that Win11 is currently under investigation and not yet official supported
ok…good point
thanks Oliver for clarification.
Any update @oliver_D ? Which is the status of the investigation?
Thanks
Ciao
Valerio
Thanks @kovarj ,
I have found your post: Windows 11 compatibility of SafeDESIGNER - Share Info & Ideas / How-To & Wikis - B&R Community
It’s weird we have 4 posts for the same topic
Thanks
Ciao
Valerio
4 posts for the same topics?