Time Data type Variable not loading

Hi, I am currently using AS 4.12 and am trying to load Values from XML into a variable via the Recipe Configuration Method. I am able to write the values of the variable for all data types except the “TIME” Data Type variable. It is always showing as T#0MS. I have tried the values T#1S, T#1000MS, T#1M, but the values in XML are not reflected. Am I missing something? Why is only the TIME data type is not working, while all other data types like Real, DINT, USINT, and STRING are working fine? Attached sample XML File for reference.

Can you try to change MS to ms?

Property ID=“Var4” DataType=“TIME” Value=“T#100ms”

Hi, thanks for the reply. Tried changing to ms, still the same error.

What is the data type of variable declaration? Can you share a printscreen from the declaration? Can you reduce your example to only one node of this TIME datatype?

Hi,

Please find the Declaration Part.

I did simple test in Automation Studio 6 and result for single variable of type TIME is:

you can do the same test, just delete xml file, and execute command save. It will create new file in proper XML format.

Ok, We have to put input of Numeric values alone. Can’t load the prefix “T#”. I tried the numeric value; it is working now.