Having an issue with transfer to PLC reporting properties are invalid. The help for the error suggests it is due to transfer properties / settings are invalid. All settings I am aware that affect the transfer are at default. This is an existing site where we have transferred many times (over 10 years - we did upgrade the PLC CPU around 12 months ago). This site uses AS4.11 with PLC OS D4.92 which is a combination we have installed is many sites without issue. The PLC CPU has also been powered cycled numerous times.
i don’t know the issue. But if your still on site and in need of a alternative solution i would suggest to try to bring the PLC in Service Mode before Transfer.
My colleague just had another opportunity to try again when production was stopped this afternoon. One plc restart and then he tried the transfer. Received a different error today than I did yesterday.