Hi, Is there a way to turn the USB port on and off via the PLC program?
Hi,
not as I know.
But as long as you’ve no code running using the USB port (for example code based on AsUsb + FileIO or DvFrame libraries), the port has no function except of the built-in functions.
These built-in functions are:
- detecting and using a B&R hardware dongle (1TG…)
- using a USB mass storage device by a static defined file device inside the Automation Studio project (this is configurable in the AS project by the developer)
- initial installation of a PLC with a USB stick containing a valid project structure prepared by Automation Studio
Best regards!
Thank you Alexander,
I am running the Raspberry Pi device via the USB port of the PPC2200 PLC and it would be nice to be able to turn its power on and off whenever I want via USB.
Best regards!
Hi,
ah ok, now I understood, your question is not about security ![]()
So unfortunately I don’t think it’s possible.
Best regards!