VC4 Alarm widget with Axis Errors

Greetings, colleagues!
While dealing with the signaling system in VC4, I noticed that when working with axes generating several errors, it is impossible to acknowledge them one by one.
I used an example from the Coffee Machine project.

Could you please tell me what are some ways to correctly combine alarm system and axes errors?



Can you please explain the problem you have? In the code above I see no interaction between the axis and the alarm system other than your mockup.
If an alarm can be acknowledged while it is active (alarm image index is still 1) depends on the settings you made for this alarm in the alarm system.

See AsHelp GUID: d7e8db93-f489-484f-97e9-04d09712a242

Hi @Pavel_Bezrodnyi do you still need help with this issue? If so, can you please reply to Christian’s question?