Version mismatch. Module mtfilter has version or date V5.24.1 instead of required range from V5.12 up to V5.12. 425

I am using AS version 4.12.3.127 SP.

Updated the old software from svn in my new laptop then this issue is coming.

V5.12 up to V5.12 versions not available in website.

Followed few steps.

 1. Update MTFilter library 
  1. Delete MTFilter and again add it from B&R library issue not resolved.

How to resolve this issue

Hello

In any case I would recommend to used latest Service Pack => AS 4.12.9.

What means you updated old software?

MtFilter is part of mapp Controls.

Can you provide a screenshot of Project / Change Runtime Versions?

Do the mapp libraries (versions) in software configuration (CPU.sw) match the versions of mapp TPs selected in Project / Change Runtime Versions?

mapp Controls 5.12: V4.3 TP Upgrade (mappControl_5.12.0.7) | B&R Industrial Automation

Lg Michael

Hi,

Thanks for your reply

find screenshot of change run time versions

Hello

Please check software configuration => CPU.sw, which version of MTFilter do you see under Library Objects and which version of MpControls is installed on you system? This needs to match.

Lg Michael

Hi,

MTFilter 5.24.1

acp10cfg 5.31.0

version installed

Hello

Try to perform a clean configuration / rebuild.
Also please try to use newest AS 4.12.9 SP.
You are sure you have MpControl 5.24.1 installed correct?

Besides that running a bit out of ideas, so might be necessary as a next step to quickly check with your local support.

Lg Michael

Hello,

if you get an Dependencies conflict, it is important to look which File has caused the issue.
The Message output does have a Colums File which could be moved to the far right and therefore unvisible by not scrolling.

See Example of a Coustom Library Dependencies Error.
It tells that “operator” has wrong version, but the cause was “Library”

Greetings
Michael Bertsch

Hi all,

Thanks for your support.

Followed below steps

  1. mappview 5.12.1 installed
  2. ACP10 ARNC0(Motion) 5.31.0 version updated in runtime versions

then issue resolved

Thanks

Veeresh