Where is BR.AS.LibraryExporter.exe documented

Where can I find this?

Is this a bug in AS Code update function?

Now 6.5 is installed but when I search in

I don’t get any result for

  • DependencyFilePath
  • LibraryExporter

:frowning:

I wanted to see the format of the exported file

→ is it for SBOM (CycloneDX)?

Where can I find this?

Help GUID d750bdd3-0aad-4486-8c0d-4eb43372b325

Thanks, but that doesn’t seem to be related to the newly implemented function/command-line application. The table shown isn’t on the GUID page.

The page mentioned is for manual export and isn’t something that can be automated.

Do you have the AH 6.5 ?

This should be the info: projectorganisation_logicalview_libraries_exportsourceasbinary.pdf (85.9 KB)

Thank you very much.

I’m still little bit confused about AS Code Workflow:

  • AS Code → Tools → Check for Updates…
    → did not give me “6.5”
  • B&R Downloads → 6.5 → newly installed
    → Help was not installed for this version

Did not know that when I install “AS 6.5” the “AS Help 6.5” is not installed or an old version is installed.

Did not know that when I install “AS 6.5” the “AS Help 6.5” is not installed or an old version is installed.

They changed the package that the AS installation is not that big in size and only the minimal parts are included.
So yes, you have to download the help separately or update it with Tools→ Upgrades from within AS. ( Same with the Automation Runtimes.. AR6.5.1 should be downloaded/updated on a second step.