Which post processor should I use in solid works so that the B&R controller can interpret the G-code?
Hi,
I don’t know SolidWorks but I guess it can output G-code.
The B&R CNC interpreter supports two flavours of G-Code:
Comparison of G-Code programming languages
‘G-code Alternative 1’ should be mostly compatible with Siemens.
Thanks for you’r answer! I will try a post processor from Siemens.
Hopefully it will work.
Hi,
could you meanwhile solve your usecase? If Yes, can you mark the Thread as solved, or even better, descripe how you did it.
I may add that we also have a possibility to adopt the B&R G-Code interpreter and that there is expirience for example to adopt it to “Bachmann”, “3D-Printing” Syntax aswell.
Greetings
Michael