I’m using X20DS1119 and an external encoder on my project to read conveyor speed, and then make the encoder as a Acp10 axis so that I can synchronize my servo motor with the conveyor, but I don’t know how to configure the X20DS1119 and the Acp10 axis.
Start looking at this block. MC_BR_InitReceiveNetworkEnc
Otherwise if you find your conveyor encoder signal is very rough/coarse, you can do more filtering (than is available in the drive) on the PLC and use a simple cyclic velocity or position to command the axis.
Correct. You don’t need to set up a SDC axis for this block.
For this block, you are setting up the data to be read from the device directly from network.