Hi,
I try to generate impulse acording the position of an axis by using a X20DS4389 Module and the fb ASMcDcsPrecisionDigitalCamSwitch from the ASMcDcs Library.
I think the function bloc is working like my expectation. If I trace HwOuput.Sequence I see the value increasing on the corresponding position of the axis.
I see also the Timestamp changes cyclicaly.
On the X20DS4389 itself I see the double flash on the “e” LED :
• Oversample output control error
• Oversample output copy error
I imagine it is a problem in the my configuration.
On this you can see the configuration of the board.
Thanks for your help