2 X90 in a AS project

Hi,

is it possible to have two X90CP174 controler in the same AS project? If yes, how?

Hello,
you can have more configurations in the project. You can find the procedure of adding configuration in the help.

Hi Pavel,
I know that I can have several configurations in one project. Maybe, I asked the wrong question.
I have to have more than one controler in the same network, like B&R reduncay solution. But it seems, it is unfortunately not possible with X90.

You can work with an X90 as a controlled node:
AH: iCN

This is then a controller acting as a powerlink slave but running its own tasks and controlling his onboard IO locally. This is not the same as a redundant system but it might be what you need.

Hi Jan,
that sounds good. Will check this.
Thx