I have my Visualization in the mappviewcfg:
but no Link in the CPU config, so it doesnt start on the panel. only Boodmode : RUN
How can I link it?
Thank You!!!
Hi @Martin_Szilagyi1 ,
very interesting question… ![]()
At the moment, mapp View embedded is not officially released yet, though it will be soon. I’m sure R&D is working on some great demos for us, so with the information we have today, I’m not sure how much the Community can help with this.
@hobi72 we need your help ![]()
Ciao
Valerio
I thought you alread solved it. 4PPC650 after transfer project only Boot mode : RUN - #4 by Martin_Szilagyi1
yup we have 2 posts for the same key question: How can we use mapp View embedded on 4PPC650?
Unfortunately mapp View embedded is not available at the moment.
We should merge them in one ![]()
mapp View embedded is so far not publicly available - only as Engineering Sample.
Everyone having / using this Engineering Sample should have an official contact for problems. In “worst case” the person, he received the Engineering Sample from … I’d recommend to contact this person.
Hobi
How did you create your mapp View EMB HMI?
Usually, if you have an PPC650, you add “mapp View” - during this process you should have had the choice to use “embedded” hardware" or “brease hardware”. The correct choice here would be “embedded” … this should create the mapp View HMI (based on the selected template).
(in my screenshot, I have already one embedded HMI connected to my PPC650).
That’s pretty much everything.
You can check the hardware configuration:
If you have only one HMI, “Visualization name” can be empty - if you have more than one, select the desired one.
If “mapp View Embedded” element is missing, please update your HWX files.
Hobi
Thanks so much for the clarification @hobi72 !
Ciao
Valerio
Hi,
I only have the Evaluation Version of AS6 and the C650 panel.
My mapView Version is 6.6.0.1 and I’m not able to update.
maybe that’s the problem…
Thank You!
Martin
I downloaded mapView 6.8.2.1 and now I get the Error 701
6 Warning 20/11/2026 17:48:31,0423 System.ArgumentOutOfRangeException has been handled, calling ISoftwareCatalogElement.ShowWizard on instance of class BR.IAT.ApiAdapter.Software.MappViewSolutionElementAdapter from C:\Program Files (x86)\BRAutomation\AS6\AS\TechnologyPackages\mappView\6.8.2\bin\Adapters\Api6.0\BR.IAT.ApiAdapter.6.0.dll. 701
What can I do now?
THX
martin
Hi @Martin_Szilagyi1 ,
actually that is a warning not an error.
Please try the sequence:
1.Close AS
2.Go to your prj folder
3.Delete Temp + Binaries + Diagnosis folders
4.Open AS
5.Open your prj
6.Project > Clean Configuration…
7.Project > Rebuild configuration
Do you still see the warning?
Ciao
Valerio
After a restart of the laptop I’m able to insert mapView but I’m still not able to choose embedded mapView…
Hi Martin,
as Christian and Pavel said you don’t have installed yet mapp View embedded, so you can’t find the new settings available in the engineering sample.
Call our B&R office in your area and ask for that engineering sample.
Ciao
Valerio
I did it already!
Thank You!
Martin
ok Martin,
I didn’t use that so far, but as Christian said you should have an official contact for problem, that contact is not the Community.
Ciao
Valerio
Since there is no official release of this, the community cannot help. The discussion is closed because there is nothing we can do now.