The B&R 8I66S200037.0P-000 module, and the 7-segment display on the front of the module is completely OFF.
Checked the PLC project and found that this module is currently disabled/not activated in the hardware configuration.
Question is:
If the module is disabled in the configuration, is it normal for the 7-segment display to remain OFF, or should the display still power up and show a status/error code? I’m trying to determine whether this behavior is expected due to the configuration or if the display/module itself may be faulty.
Additional observations:
- The module is powered.
- The S/E LED shows a repeating pattern: ON → 3 blinks → OFF → repeat.
- Communication with the interface module is not established.
Has anyone experienced similar behavior with the 8I66S200037.0P-000?