Acopos 1045 and Servo Siemens

Hi everyone, I’ve run into an issue — perhaps someone has tried doing something similar.

I want to connect a Siemens SIMOTICS S 1FK7042‑5AF71‑1AA0 servomotor to an Acopos 1045. I have the ac122 module for the resolver, and the servomotor itself also has a resolver.

I’ve made a resolver adapter, and in the system, when you manually turn the shaft, you can see the coordinate changes.

Here’s the problem: when I turn on PowerOn, the shaft twitches slightly and then throws errors 38005 (Motor test: Speed is too high during switch on) and 4007 (Lag error stop limit exceeded).

Could you suggest what I could check or do? I’ve double‑checked all the connections, the motor phases, and the resolver cables several times. I’ve entered the motor data according to the manual.

Hello,

Have you checked this topic? It’s definitely helpful.

  1. Thank you for the link to the topic — it really helped me solve my problem.