Acopos multi i005d servo drive not powering

Why my acopos multi i005d servo drive not blinking any led lights or not getting power while other servodrives are all working and blinking lights ?
what could be the reason for the acopos multi i005d not working?
what can be done to resolve this issue

is there anyone who can help @Darwin?

One known typical Issue:
The ACOPOSmulti has a Backplane which supplys the DC-Bus and the 24V-Bus. The Module connects to the Copper-Rails via a Clamp, which is actuated by the bottom fixing Screw. This Screw must be actuated with a spezific torque to ensure correct connection between the Module and the Backplane.

So if all Modules left and right of the one are active and only one in the middle is not active, maybe unscrew and screw the Module again.


If the Module has still no lifesignes after this test, its probably best to contact local Support. Because the module might be damaged.


If you are an electical capable person you can supply the module by a 24V-laboratory Power-Source for testing. But i would not recommend this if you are not knowing how to do it safe.

Greetings
Michael