Acopos P3 SafeMotion Problem SE LED constantly on

Hello,

I have three Acopos P3 SafeMotion, two 8EI034HWSS0.0200-1 and one 8EI017HSS0.0600-1, and two works fine, but one (8EI034HWSS0.0200-1) has some problem, the LED SE is constantly on. I installed the latest version of the SafeMotion hardware module and AcoposP3, but it did not help.

It has been doing this since the first power up.

I am using AS (4.12), Safedesigner (4.4.1), ACP10/ARNC0 5.29.1, mappSafety 5.24.1, AR P4.93, the main controller is 4PPC80.101E-10A.

From logger:

Hardware config: