Hello,
we have an old project developed with AS 3.0.90 with ACP10 version 2.32.2.
We didn’t found ACP10 2.32.2 for AS 4.x. Is it available?
We wouldn’t update ACP10 version if possible.
Thank you very much
Regards,
Giovanni
Hello,
we have an old project developed with AS 3.0.90 with ACP10 version 2.32.2.
We didn’t found ACP10 2.32.2 for AS 4.x. Is it available?
We wouldn’t update ACP10 version if possible.
Thank you very much
Regards,
Giovanni
Hi,
I don’t know the exact version dependencies of ACP10 packages and Studio versions.
But in general, because of some legal dependencies, older versions were removed from the download section.
Please contact your local B&R support / office to check, if and how it could be provided.
Best regards!
Hi @Giovanni_Boschello ,
feedback from R&D:
we have ACP10 2.32.2 upgrades for AS2 and AS3 but not for AS4.
Ciao
Valerio
Thanks @valerio.manenti
Which version is the most near to ACP10 2.32.2 usable for AS3 and AS4?
interesting question…Do you want to support the old powerlink AC112 cards?
Few details I got from Support last year:
”when the customer has a machine which is using a combination of AC112 and AC114 then they need to use PLK V1 and need to stay on ACP10 V2.xx.x versions otherwise AC112 won’t work anymore. The latest version in the ACP10 V2.xx.x family is V2.52.8 indeed. This is “so far” away from V3.xx.x because we simply made a version jump with ACOPOS P3 to V3.xx.x Similar to the jump we made from ACP10 V3.18.2 to V5.xx.x and the jump we are going to make from V5.27.x to V6.xx.x”
Ciao
Valerio
Hello Valerio,
we just need to support 8AC114.60-2 (the powerlink V2 module).
We have also 8AC120.60-1 (Endat 2.1) inserted into the ACOPOS 8Vxxxx-2.
Thanks
Hi @Giovanni_Boschello ,
for example i’ve found 2.37 for both AS versions: