Motion Acp10_V1.210 Does anyone can provide it?

I have an old project originally build with AS version 2.5.3. Unfortunately I can only installed AS version 2.7 on my window 7 laptop. Now, it got complied error with
“acp10ext:Error:1012:Error text file for ‘acp10’ software version ‘1.210’ are not installed. Install version ‘1.210’ of ‘acp10’ software or change version in the project.”

I think I need to install acp10 v1.210. Does any one can provide it ?

What is your purpose to use such an old Automation Studio and ACP10 Versions?
If you want to change something on the machine, I would suggest to migrate to some newer versions, at least to AS 2.7.
For just diagnosis purposes you could also use some newer versions and try to read the information you need, without a transfer of the project.

Yes, I need to change something on machine and I agree that it’s better to migrate to AS 2.7 as you mention. Now, I got error as above. I expect that I need to install that acp10 V1.210. or how can I solve this ?

I would try to switch to an ACP10 version which is installed in Automation Studio 2.7. In my AS2.7 there is ACP10 2.42.2 pre-installed.
The older the AS version is, the harder it is to get some upgrades or do any other stuff.
Depending on what you need to change, the lifecycle of the machine and so on, I would also recommend to switch to newer AS versions.

Hi,
I agree with Samuel, it is probably easier to change to a newer version.
There is also another hurdle, because Acp10_V1.210 is subject to the dual-use export restrictions per Regulation (EC) No. 2021/821 of the European Community.
To get this version you have to contact the Support office for your country: Locations

Thank you for your reply.

You can change the version here:

Thank you again for your reply, problem with acp10 now solved. I have next question due to visual component.

During migrate project it asked for upgrade visual component SG3 from version 01.63 (actual used in project) to newer version 3.63 (preinstalled with AS2.7).
I did upgrade because I don’t have VC3 V01.63 installed
.
Then during complied project, it asked for update visapi library from V2.54.2 to 3.35.2. I click cancel to leave visapi library as it is.

Now, project successfully complied and able to generate CF but I am not so sure if I did it right. The machine’s B&R component is very old one. I also a bit worry about compatibility for those update.

What do you think ?

By the way, If I update visapi library to V3.35.2, it result in FATAL error as below.

"FATAL error: Module visapi version mismatch. The time or version of this module is V3.35.4. It is accepted only from V2.52.2 up to V2.54.2 in dependency of module hmi_lib "

Hi Siripon,

this message propably comes from library “hmi_lib”, which should be a user-library and no official B&R library. In this lib there should be some dependencies manually added. It should work if you remove these dependencies.