We are currently using X20CP3686 - Redundant PLCs.
We are using 5 RIO’s, We have to add additional RIOs for the same CPU. Can we add those without Downtime.
We are currently using X20CP3686 - Redundant PLCs.
We are using 5 RIO’s, We have to add additional RIOs for the same CPU. Can we add those without Downtime.
Hi,
I’m not sure about “RIO” - do you mean Remote IOs?
If yes, it depends on if the Remote IOs are already configured in the project but just not connected - if yes and you’re using a fieldbus with hot-plug capabilities (like powerlink), then you can add them.
But if those IOs aren’t configured yet in the project, you have to add them first on project software side. Unfortunately, I don’t have experience with redundancy, but looking into the project installation sequence for redunant systems, at least it looks like that it could be possible by updating first the non-active PLC - but as I said, I’m not so familiar with CPU redundancy, so I’m not sure about:
Best regards.
Closed by moderator due to inactivity.
For others, if you want to help from the Community, you have to continue the discussion and update the status of your progress. Otherwise, it is hard to help you.