APC3100 to Desktop Monitor connection for Visualization screens

APC3100 acting as PLC, Connected DVI cable from APC3100 to monitor but visualization screens are not displaying in monitor how to configure normal desktop monitor in APC3100

In an embbeded system, you can create a visual components visualization, which can be shown on the local connected screen.

https://help.br-automation.com/#/en/4/visualization%2Fviscompvc4%2Fvisualcomponents_overview.htm

Thanks for your reply
Visualisation screens created and program dumped to APC3100 & APC connected to normal desktop monitor, I can be able to browse Visualisation screens in my laptop using VNC server(connect via target APC ) but screens are not shown in normal desktop monitor connected to APC.

You have to insert an Automation Panel to the Monitor/Panel interface of the APC3100 with the same resolution of you external screen. Then you have to link the VC Visu with the same resolution to this Automation Panel.

In this example : VGA → 640x480 resolution

Added VC4 1920*1080 program & connected dell monitor U2722D QHD 2560 x 1440 monitor to APC via DVI-D–HDMI Cable then which automation panel should I add to monitor/panel configuration & what are the cables should I connect from APC to monitor.

Any AP screen with FHD would work.

image

Thank you.
How should I install the USB & keyboard drivers for this APC3100 because no OS installed in this PC.

First you have to add in the physical view an usb keyboard.


In the configuration in the VC folder you have to define the keys for the USB-Keyboard.dis file.

You have to define the numbers TP_ALPHA_0 - TP_ALPHA_9, TP_ENTER, TP_TAB, TP_BACKSPACE and so on.

Hi Veeresh, what is the status of your topic, have you find solution? can you update us and mark reply with solution? thanks Jaroslav

Thank you for your support