AR transfer is taking too long

Hi Everyone, I’m having issues while transfering the AR to a 4PPC30.


It usually takes around 5 minutes but now it’s been like 55 minutes and the CPU is still restarting multiple times.
I’ve already stopped the transfering and starting again and still the same issue.
Please, i’d like some advices. Greetings.

It appears that you have transferred the AR without the sysconf / arconf modules from the project. Therefore the system does not currently have an IP configuration and will have booted with DHCP client option.

You can press cancel and then find the current IP or set the IP using the “Browse for targets” option in the Online settings.

You could also create a USB install stick, connect it to the PLC and then boot into BOOT mode by pressing the reset button in sequence. This will install the project.

  1. Press key briefly (<2 s)
  2. Pause (<2 s)
  3. Press and hold key (>2 s)

See AsHelp GUID: 65deab54-ffa2-4922-b7d3-c1208c7970dd

I’ve already tried using the USB installing method but didn’t work either. Also I change the AR version and nothing changed.
I checked that the sysconf / arconf modules were present on the Configuration Objects and they were Ok, thank you for your suggestions.

My solution was to create a new configuration and drag and drop all my tasks, libraries, IO mappings,visualization ,etc.

I’m not sure of what happened, maybe the configuration was corrupted in some way.

Generally I am skeptical about behaviors which are attributed to “corruption” as it does not explain anything. It would be interesting to compare the source files between the “good” and “bad” configuration to see if there are settings which are different or have been forgotten. It would also be interesting to download the “bad” configuration to the machine again to see if this behavior is really consistent with the configuration however I understand that you do not have time for this.

What I meant with “you forgot to include the system configuration files” is not that they are present in the software configuration but that when you do a bootstrap loader OS update only the OS is transferred and therefore without IP configuration unless you select during the update the option “Modules from the project scheme”. Only then will the OS boot with the IP configuration from the project.
See AsHelp GUID: 0bcc17ff-31b1-4855-a0a3-355764af5f73