AR V2.92 for 7EC021.61-1

Hello,

I need to make minor change in the application at 7EC021. Original project uses V2.92, but I have Q2.96. I would like to keep AR version the same as it is. I was looking at B&R site but I can’t find it. Do somebody have it maybe?

Thanks,

Hi @Matjaz_Kopac ,

it looks like we had the same question here: V2.92 download software - Ask Questions / B&R Software & Runtime - B&R Community

TLDR: this version was bundled with AS 2.6.

Thank you for answer. I went to that topic but it seems no more old SW is available anymore. Oldest AR available there is for AS 4.7. I would also ask our country (Slovenia) support but the only person employed there is on a vacation… I’ll try getting support in Prague.

if you do not reach support, let me know and I will ask someone in y our region to help you.

I received from tech support in Brno versions D2.92 and C2.92 right now… But I think this will not help as we need V2.92. Maybe would be easier if I change the project version to Q2.96? But then the others who have access to this CPU and have installed AR V2.92 will have to make upgrades as well…

you need exact version of AR, for sure..

Hi,

I sent you a private message with V2.92 upgrade out of AS2.6 for AC140 (regarding to the homepage, 7EC02x is based on operating system AC140).

I downloaded it. Thank you!