Some time to time during development of network related features it’s useful to have ARsim accessible from other PCs or devices of the local network.
Known solution is to set Simulation IP in PLC configuration to the local Windows IP.
There is a better and more flexible solution that will make it possible to reach the ARsim services from local network even if the local Windows IP changes.
The solution is smart and straight forward, just set the Simulation IP to 0.0.0.0 and it will work locally on localhost and on local windows IP over the network.