AS6.5 installation fails with error (AdminByRequest is used)

Hello

I have a lots of problem trying to install AS6.5..0.306

Doing uninstall-install lots of time

Some time installer run up to end, but i get random error 701 when trying open mappView page

2025-12-22_18-48-27

Some time installer show “complet” but still doing stuff

Some time, at AS start, I get this

I am using “AdminByRequest” to install AS6.5

I feel like ABR do not assign full admin level and some part are not well installed

Can you help me ?

Thanks

Marc

At the company I work for we also had Admin By Request. We also had a lot of problems installing automation studio (AS5.X.X) and the IT therefore decided to remove Admin By Request and to search for an alternative.

.agree. as alternative you can use virtual mechine with full rights.

@Marc_Pinchart
I checked in AS Help 6.5.1.3 some information about AS 6 and virtual machine and unfortunately I saw an interesting note:

Ciao
Valerio

Thanks … this is interesting

I try on VM with full admin (no ABR, Win 10), It seems it is working …. except, i still have trouble with the text system (see “Text AS6”)

Marc

I think this is more of an issue running ARsim in a VM as an Automation controller for testing/ModbusTCP control.

I’ve worked with customers using Automation Studio from 3.0.90 and later in VMs. The biggest issues we run into is if the VM is trying to access files on the host machine and not in the VM.